- No : 22507
 
      - Release Date : 2018/09/03 17:28
 
        - 
          
              Print
          
        
 
  
 
GX Works2's USB driver installation procedure
    
      Is the USB driver installed along with the installation of GX Works2?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    The USB driver is not installed.
The driver needs to be separately installed before the first connection to a CPU module.
  
    
      
        - Product Name
 
          - MELSEC-Q Series
 
      
      
        - Series
 
          - Software Package (GPP function)