• No : 22507
  • Release Date : 2018/09/03 17:28
  • Print

GX Works2's USB driver installation procedure

Is the USB driver installed along with the installation of GX Works2?
Category : 

Answer

The USB driver is not installed.
The driver needs to be separately installed before the first connection to a CPU module.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)