• No : 22522
  • Release Date : 2018/09/03 17:28
  • Print

PLC type change in GX Developer

The PLC type cannot be changed in GX Developer. Are there any remedies?
Category : 

Answer

Follow the steps below and then execute PLC type change.

- On the menu of GX Developer, select [Online] -> [Monitor] -> [Stop Monitoring (All Windows)], to stop all monitoring processes.

- From [Window] on the menu of GX Developer select the device batch monitor window, the entry data monitor window, and the buffer memory batch monitor window and close all of them.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)