FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
>
How to use file registers R in the Q ...
Back
No : 22525
Release Date : 2018/09/03 17:28
Update : 2018/09/20 14:29
Print
How to use file registers R in the Q series
File registers set in units of 64k points are used in the Q series.
Can file registers R be used only for data whose size is up to 32k points?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
Answer
File registers R can be used for data whose size is exceeding 32k points with RSET instruction, which is a block switching instruction.
Use file registers ZR if serial device numbers are desired.
Product Name
MELSEC-Q Series
Series
Q (Q mode)