• No : 22525
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 14:29
  • Print

How to use file registers R in the Q series

File registers set in units of 64k points are used in the Q series.
Can file registers R be used only for data whose size is up to 32k points?
Category : 

Answer

File registers R can be used for data whose size is exceeding 32k points with RSET instruction, which is a block switching instruction.
Use file registers ZR if serial device numbers are desired.
 
Product Name
MELSEC-Q Series
Series
Q (Q mode)