• No : 22581
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 17:12
  • Print

Sample comment of GX Works2

Does GX Works2 include sample comments?
Category : 

Answer

It includes sample comments for special relay/special register and the intelligent function module.

On the menu of GX Works2, select [Edit] -> [Import from Sample Comment]
-> [Special Relay/Special Register] or [Intelligent Function Module] to import the comments.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)