• No : 22614
  • Release Date : 2018/09/03 17:29
  • Print

Error code "2200" in the universal model QCPU

The error code "2200" has occurred in a universal model QCPU module. Are there any remedies?
Category : 

Answer

The error code "2200" is "MISSING PARA.".
The cause of the error is that a parameter file does not exist in all drives where parameters will be valid.
As a remedy, write a parameter file into a PLC drive to be valid.
Product Name
MELSEC-Q Series
Series
Q (Q mode)