- No : 22645
- Release Date : 2018/09/03 17:29
-
Print
Accessing file registers from the built-in Ethernet port QCPU using A-compatible 1E frames
Is it possible to access file registers from the built-in Ethernet port QCPU using the MC protocol's A-compatible 1E frames?
- Category :
-
Answer
The QnUDE(H)CPU modules with serial numbers with upper 5 digits of "14112" or later indicate compatibility with the function. The accessible device range is from R0 to R8191. The High-speed Universal model QCPU (QnUDVCPU) does not support the function.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)