- No : 22736
- Release Date : 2018/09/03 17:29
-
Print
CPU clock setting by SNTP functions via built-in Ethernet port in LCPU
Is the CPU time set automatically by the time setting function (SNTP client) via the built-in Ethernet port in the L series CPU?
- Category :
-
Answer
The clock setting of the CPU module is set automatically in accordance with the clock data collected from the time information server (SNTP server) on the LAN.
- Product Name
- MELSEC-L Series
- Series
- L Series