• No : 22736
  • Release Date : 2018/09/03 17:29
  • Print

CPU clock setting by SNTP functions via built-in Ethernet port in LCPU

Is the CPU time set automatically by the time setting function (SNTP client) via the built-in Ethernet port in the L series CPU?
Category : 

Answer

The clock setting of the CPU module is set automatically in accordance with the clock data collected from the time information server (SNTP server) on the LAN.
Product Name
MELSEC-L Series
Series
L Series