- No : 22772
- Release Date : 2018/09/03 17:30
-
Print
Simultaneous broadcast reception setting for built-in Ethernet port LCPU
How do I configure the setting to receive simultaneous broadcast during socket communication of L series CPU with built-in Ethernet port?
- Category :
-
Answer
To receive simultaneous broadcast using UDP, set the parameters as follows.
- Destination IP Address: FF.FF.FF.FFh
- Destination Port No.: Other than FFFFh (Receives the data sent from the specified destination port number.)
: FFFFh (Receives the data sent from all destination port numbers.)
- Product Name
- MELSEC-L Series
- Series
- L Series