- No : 22775
- Release Date : 2018/09/03 17:30
-
Print
Maximum number of connectable modules to LCPU when it is not extended
What is the maximum number of modules to be connected without using an extension/branch module?
- Category :
-
Answer
Up to 10 modules can be connected in the system as a whole except for the power supply module, CPU module, display unit, RS232C adapter, and END cover.
Some modules take up the space of two modules. Refer to the manual of each module.
- Product Name
- MELSEC-L Series
- Series
- L Series