- No : 22783
- Release Date : 2018/09/03 17:30
-
Print
SNTP communication error in built-in Ethernet port LCPU
When the time setting function (SNTP client) is used in the L series CPU with built-in Ethernet port, is the CPU time affected if an SNTP server communication error occurs?
- Category :
-
Answer
The error does not affect the CPU time. The CPU time is not set when a communication error occurs.
- Product Name
- MELSEC-L Series
- Series
- L Series