• No : 22783
  • Release Date : 2018/09/03 17:30
  • Print

SNTP communication error in built-in Ethernet port LCPU

When the time setting function (SNTP client) is used in the L series CPU with built-in Ethernet port, is the CPU time affected if an SNTP server communication error occurs?
Category : 

Answer

The error does not affect the CPU time. The CPU time is not set when a communication error occurs.
Product Name
MELSEC-L Series
Series
L Series