- No : 22810
 
      - Release Date : 2018/09/03 17:30
 
        - 
          
              Print
          
        
 
  
 
LCPU protection function
    
      Can I set a password to protect LCPU programs so that it acts like a black box?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    A password can be set. 
- Use the file password 32 function.
- Number of characters: 4 to 32 (alphanumeric and special characters, case-sensitive)
- Disabled operations: Write, read, read/write
- Target: Programs (program files), parameters, device comments, initial device values, symbolic information
  
    
      
        - Product Name
 
          - MELSEC-L Series
 
      
      
        - Series
 
          - CPU