• No : 22816
  • Release Date : 2018/09/03 17:30
  • Print

CPU built-in I/O function

Can I use the CPU built-in high-speed counter function and positioning function simultaneously?
Category : 

Answer

They can be used simultaneously when I/O signals are not overlapped. The overlap of signals are checked automatically when a user select functions in the built-in I/O function parameter setting window.
Product Name
MELSEC-L Series
Series
CPU