• No : 22825
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/27 11:38
  • Print

L60DA4 accuracy

What is the accuracy of L60DA4?
Category : 

Answer

- Ambient temperature: 25+/-5 degrees Celsius with tolerance of +/-0.1%
- Ambient temperature: 0 to 55 degrees Celsius with tolerance of +/-0.3%
  (accuracy for the maximum analog output value)
Product Name
MELSEC-L Series
Series
D / A Conversion Unit