- No : 22835
- Release Date : 2018/09/03 17:30
-
Print
Operation performed when file registers are read
Are file registers read if "Device memory" in the Read from PLC window of GX Developer/GX Works2 is checked? (Standard RAM, created in the following file format)
- Category :
-
Answer
Checking "Device Memory" does not read file registers. Switch the Target Memory for "PLC Data" to "Standard RAM" and check "File Register" in the Read from PLC window to read file registers.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)