• No : 22845
  • Release Date : 2018/09/03 17:30
  • Print

Accessing a QnA compatible Ethernet interface module via a router using GX Developer

Is it possible to connect GX Developer to a QnA compatible Ethernet interface module via a router using the Ethernet adapter on the personal computer?
Category : 

Answer

For GX Developer, a connection via a QnA compatible Ethernet interface module allows communication only within the same segment. Via a router, it is impossible to access programmable controller CPU modules within other segments via a For QnA Ethernet interface module.
Product Name
Engineering Software
Series
Software Package (GPP function)