• No : 22859
  • Release Date : 2018/09/03 17:30
  • Print

A message that says "A T/C coil with the same No. exists."

When a project is saved under a specified name, a message appears, stating "A T/C coil with the same No. exists in the program (MAIN) or program (MAIN-SFC). The set value is changed to that for the first T/C coil.". What does it mean?
Category : 

Answer

It is a confirmation message telling a user that there is a device, T or C, that has become a duplicated coil in the same program and the coil is given the set value for the first set T/C coil.
Product Name
Engineering Software
Series
Software Package (GPP function)