• No : 22861
  • Release Date : 2018/09/03 17:30
  • Print

Reading project data from a CD-R

Project data of GX Developer on a CD-R cannot be reopened after the data is written to the CD-R. How can I read it?
Category : 

Answer

To reopen project data written to a CD-R, copy the project data into a space such as a hard disk on the personal computer where the project data is used.
This operation is required because GX Developer executes data writing when a project is opened.
A project folder copied into a HD is set to "read only". Uncheck the "read only" box.
Product Name
Engineering Software
Series
Software Package (GPP function)