• No : 22872
  • Release Date : 2018/09/03 17:30
  • Print

Writing QJ71C24N's parameters in GX Works2

When are the switch setting and the settings of "Various Control Specifications" for the QJ71C4N series intelligent function modules written by GX Works2?
Category : 

Answer

The switch setting is written when CPU module's parameters are written. The settings of "Various Control Specifications" are written when intelligent function module settings are written.
Product Name
Engineering Software
Series
Software Package (GPP function)