• No : 22873
  • Release Date : 2018/09/03 17:30
  • Print

GX Works2's compatibility with the ACPU modules

Does GX Works2 support the ACPU modules?
Category : 

Answer

GX Works2 does not support the ACPU modules.
Use GX Developer for the ACPU modules.
GX Developer is included on the CD-ROM of GX Works2.

For the installation procedure, refer to the following manuals.

GX Works2 Version 1 Operating Manual (Common)
Model code: 13JU64
Appendix 14 Procedure to Use GX Works2 Unsupported Programmable Controller Type
Product Name
Engineering Software
Series
Software Package (GPP function)