• No : 22893
  • Release Date : 2018/09/03 17:30
  • Print

Using send FBs/receive FBs simultaneously

Is it possible to execute multiple send FBs/receive FBs created using GX Configurator-SC simultaneously for sending/receiving?
Category : 

Answer

If multiple send FBs/receive FBs are simultaneously executed, the FBs do not function properly.
When there are multiple send FBs, do not execute two or more send FBs simultaneously. (Create a program that does not turn ON the I_START instructions for the send FBs simultaneously.)
When there are multiple receive FBs, do not execute two or more receive FBs simultaneously. (Create a program that does not turn ON the I_START instructions for the receive FBs simultaneously.)
Product Name
Engineering Software
Series
Software Package (other functions)