- No : 22943
- Release Date : 2018/09/03 17:30
-
Print
Setting a high-speed timer and a low-speed timer
I want to set the 100 ms timer for all the 256 points of the parameters of the A2SHCPU. Can I set one type of timer for all the 256 points in GX Developer?
When I use GPPA of Ver. MS-DOS, I can set 0 for the 10 ms timer and can use the 100 ms timer for 256 points of the parameters. Can I use the 100 ms timer for the 256 points in GX Developer?
- Category :
-
Answer
In the PLC parameter setting of GX Developer, delete the start "200" of the default high-speed timer and input "0". The message indicating that "There is a duplication with the low-speed timer. Do you want to delete the low-speed timer?" is displayed. Click YES.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)