• No : 22955
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/25 12:11
  • Print

I cannot select [Transfer Setup] in GX Developer because it is displayed in gray.

When I attempted to change the connection destination by selecting [Transfer Setup] of [Online] from the tool bar to start the communication between a programmable controller and GX Developer, [Transfer Setup] has been displayed in gray and I was not able to select it.
Category : 

Answer

You cannot select the item while the programmable controller is being monitored.
Execute [Close all windows] of [Window] from the tool bar, and check if Transfer Setup can be selected.
Product Name
Engineering Software
Series
GX Developer