• No : 23028
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 10:14
  • Print

Overall cable distance and station-to-station distance in CC-Link networks

How long are the overall CC-Link cable distance and the CC-Link station-to-station distance in meters?
Category : 

Answer

The overall cable distance and station-to-station distance depend on the version and the transmission speed.
Figure 1 shows the case with Ver.1.10-compatible CC-Link dedicated cables in use.

Figure1


For more details, refer to chapter 3 in the following manual.
- CC-Link System Master/Local Module User's Manual
Product Name
Network Related Products
Series
CC-Link