• No : 23037
  • Release Date : 2018/09/03 17:31
  • Print

Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function

If "Non-conversion Variable" is selected for the packet setting of the QJ71C24N series pre-defined protocol support function, which one is the unit of the receive data length of the variable, byte or word?
Category : 

Answer

The receive data length of the variable is specified in bytes.
Product Name
Network Related Products
Series
Computer Link / Serial Communication