- No : 23040
- Release Date : 2018/09/03 17:31
-
Print
Limitation on the number of levels of cascade connections when QJ71E71-100 is used
Is there limitation on the number of levels of cascade connections when QJ71E71-100 is used?
- Category :
-
Answer
If a repeater hub is used, 10BASE-T allows a maximum of four levels of cascade connections and 100BASE-TX allows a maximum of two levels of cascade connections. Ask the manufacturer about the allowable number of levels when using a switching hub.
- Product Name
- Network Related Products
- Series
- Ethernet Interface Module