• No : 23053
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 10:59
  • Print

Identifying disconnected CC-Link stations

How do I identify disconnected stations?
Category : 

Answer

Identify disconnected stations using either of the following methods.

(1) Select [Diagnostics] -> [CC-Link Diagnostics].from the menu in GX Works2 or GX Developer to identify disconnected stations.
      Clicking the "Another Station Monitor" button in the "CC-Link Diagnostics" window displays the status of each station
      in the window that appears.
(2) By monitoring the special link registers SW80 to SW83 "Other station data link status", disconnected stations can be identified.
Product Name
Network Related Products
Series
CC-Link