• No : 23054
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 11:00
  • Print

Precaution about MELSECNET/H connection (2)

What are the precautions for connecting a Q series redundant system using the MELSECNET/H remote I/O network system?
Category : 

Answer

 - Set the network module mounted in system A to station number 0 (multiplexed remote master station).
    Set the network module mounted in system B to any station number between 1 and 64.
    When the network module mounted in system B is set to station number 0, "LINK PARA. ERROR" occurs.

 - For the Network Parameters of both system A and B, set "Network type" to "MNET/H (Multiplexed remote master)".
    Also, set the system B's station number as "remote sub-master station".
Product Name
Network Related Products
Series
MELSECNET/H