- Set the network module mounted in system A to station number 0 (multiplexed remote master station).
    Set the network module mounted in system B to any station number between 1 and 64.
    When the network module mounted in system B is set to station number 0, "LINK PARA. ERROR" occurs.
 - For the Network Parameters of both system A and B, set "Network type" to "MNET/H (Multiplexed remote master)".
    Also, set the system B's station number as "remote sub-master station".