• No : 23238
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

How can I set the current value of a thermal load relay?
Category : 

Answer

A thermal load relay is set as full-load current of a motor. However, ifambient temperature is significantly different from 20℃ or the connectingwire is different from the standard wire size, it is necessary to correct theset value.
Product Name
Motor Starters
Series
MS-T/N