• No : 23249
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

How should I connect MSO-T* and MSO-N* type magnetic starterwhen using for opening/closing single-phase motor load?
Category : 

Answer

Since it is necessary to energize the pole containing a heater element of athermal load relay, you need to connect it to both side of 3 poles(Between 1/L1-2/T1 and between5/L3-6/T3).
Product Name
Motor Starters
Series
MS-T/N