• No : 23259
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What is the reason why some magnetic staters can not be usedalone?
Category : 

Answer

The temparature rise of a terminal connected by customer is designed tobe under 65℃ according to the standard. For our products, there is nospecification about connecting wire at power side terminal by customer,and therefore the heat radiation area may be smaller and it may not meetthe standard value of terminal temparature. In addition, the operatingcharacteristics is designed to operate as our catalog when combined withthe contactor. If using only magnetic starter without contactor, theoperating characteristic of our catalog may not guaranteed since there isno contactor and heat radiation could be changed.
Product Name
Motor Starters
Series
MS-T/N