• No : 23297
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

Is it possible to use surge suppressor unit UT-SA33* or UN-SA33type for a main circuit in a single-phase?
Category : 

Answer

It is possible to apply for single-phase circuit. However, it may be lesseffect in single-phase circuit (100 V, etc) since low voltage circuit is tendedto be less effect.
Product Name
Motor Starters
Series
MS-T/N