• No : 23319
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

Is it possible to produce SR-T* and SRD-T* type including a surgesuppressor?
Category : 

Answer

It is possible to produce with the coil designation of less than AC 230V andDC 220V. Please add " SA" at the end of the type name.
Product Name
Motor Starters
Series
MS-T/N