- No : 23346
- Release Date : 2018/09/12 15:12
-
Print
About Low-voltage Power Distribution Products
If ambient temperature of a solid state contactor is more than 60℃,is it possible to use it? If not, how can I deal with?
- Category :
-
Answer
The maximum ambient temparature for US-N/K/H type is 60℃ and theycan not be used with more than 60℃. If the temparature is more than60℃, you need to consider cooling inside of control panel by clearing theair with cooling fan etc. (Moreover, you need to reduce the current whenthe ambient temparature is more than 40℃.)
- Product Name
- Motor Starters
- Series
- MS-T/N