• No : 23358
  • Release Date : 2018/09/12 15:12
  • Print

About Low-voltage Power Distribution Products

What is the temperature of US-N* type cooling fins when carryingthe rated current?
Category : 

Answer

When carrying the rated current at ambient temperature of 40℃ (whencarrying the rated heater load), the maximum temparature of cooling finis approximately 100℃.
Product Name
Motor Starters
Series
MS-T/N