What happens to overlap windows when the mode is switched to screen gesture mode while an overlap window is displayed?
If the mode is switched to screen gesture mode while an overlap window is displayed, the overlap window is hidden.
The overlap window is redisplayed when screen gesture mode is disabled.
Note that in screen gesture mode, the screen switching device of the overlap windows retains the screen number of the overlap window displayed before the mode was switched to screen gesture mode.
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.