The following gestures are available for the historical trend graph.
• Swipe in the direction of the time axis: Scrolls the half the page in the swiped direction.*1
• Pinch-in in the direction of the time axis: Zooms out on the time axis by one step (Key code switch equivalent to FFF9)*2
• Pinch-out in the direction of the time axis: Zooms in on the time axis by one step (Key code switch equivalent to FFF8)*2
*1: Zooming in and out on the scale of the device value (vertical axis) with gestures is not supported.
*2: For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.