The following gestures are available for the historical trend graph.
◆ GT Designer3 (GOT2000) Version 1.100E or later
・ Tap: Displays the cursor on the tapped position.
・ Swipe along the time axis: Scrolls the historical trend graph by half the page in the swiped direction.
・ Pinch in along the time axis: Reduces the time axis by one size (equivalent to the key code switch FFF9).
・ Pinch out along the time axis: Enlarges the time axis by one size (equivalent to the key code switch FFF8).
* Enlargement and reduction in size in the device value direction (along the vertical axis) with gesture operations are not available.