Can I enable or disable single touch operation for the historical data list display with a device value?
Even when single touch operation is enabled in the historical data list display settings, you can enable and disable the operation with the device value (GS1794).
When b1 of Gesture Common Control (GS1794) is on: Single touch operation is disabled.
When b1 of Gesture Common Control (GS1794) is off: Single touch operation is enabled.
Note that when single touch operation is disabled in the historical data list display settings, this signal does not work.