• No : 23466
  • Release Date : 2018/09/14 15:06
  • Print

Object gesture function while using the GOT remote access function

Can I use the object gesture function from the VNC client while using the GOT remote access function (VNC server function)?
Category : 

Answer

You cannot use the object gesture function from the VNC client while using the GOT remote access function (VNC server function).
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (VNC server)
Series
GOT2000 Series