The following actions can disable screen gesture mode.
• Touching the screen gesture mode switch (key code: FF90).
• Touching the full scale display (100% display) switch (key code: FF91).
• Transitioning to the utility screen.
• Switching to the base screen.
• Acquisition of operation rights by the VNC client when the GOT remote access function (VNC server function) is used.
• Loss of operation rights for the GOT network interaction function.
* Place the screen gesture mode switch outside the screen gesture active area.
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.