• No : 23486
  • Release Date : 2018/09/14 15:06
  • Print

Gesture function

What operations are available for the gesture function of the GOT2000 series?
Category : 

Answer

The gesture function of the GOT2000 series includes the screen gesture function and object gesture function.

The screen gesture function allows the base screen size to be enlarged or reduced with a pinch-in and pinch-out, and the base screen to be scrolled with a swipe or slide.

The object gesture function allows the time axis of a graph or document size to be enlarged or reduced with a pinch-in and pinch-out, and a graph or document pages to be scrolled with a swipe or slide.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series