• No : 23490
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 17:33
  • Print

PLC access from GX Works3 via the GOT

When connecting the personal computer (GX Works3) and the built-in Ethernet interface of the RnCPU via the USB interface of the GOT3000 series or GOT2000 series, how should I configure the GX Works3 connection destination settings?

Category : 

Answer

When connecting the personal computer (GX Works3) and the built-in Ethernet interface of the RnCPU via the USB interface of the GOT3000 series or GOT2000 series, set the connection destination in GX Works3 as follows:

1. PC side I/F Serial Setting
• Select [USB].

2. PLC side I/F Detailed Setting of GOT
• CPU mode: Select [RCPU].
• Select [via GOT (Ethernet) transparent mode].
  → GOT (Ethernet) transparent settings
   • Model: Select [Ethernet Built-in CPU].
   • IP address: Enter the RnCPU IP address.

3. Other Station Setting
• Select [No Specification].

If the following conditions are not met, connection will not be possible. 
• Ethernet communication between the GOT and RnCPU is properly established. 
• The connection destination of the transparent function is set to RnCPU (MELSEC iQ-R, RnMT/NC/RT, CR800-D).

For details, refer to the GOT connection manual.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (FA transparent function)
Series
GOT3000 Series, GOT2000 Series