• No : 23623
  • Release Date : 2018/09/14 15:10
  • Print

Wrong connection of servo amplifier power supply

I connected the main circuit power supply (L1, L2, L3) to the servo motor power input (U, V, W) oppositely and turned the power on. Can I continue to use the system if I fix the wiring?
Category : 

Answer

The system is probably malfunctioning and is in dangerous condition. Do not use it.
For repair, contact your local sales office.

Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MELSERVO Others