• No : 23632
  • Release Date : 2018/09/14 15:10
  • Print

Long distance wiring

Can I wire the servo amplifier and servo motor in the long distance?
Category : 

Answer

For the long wiring (50 m to 100 m) between the servo amplifier and servo motor,
there are some precautions (encoder cable, etc.) to note.

The wiring is not possible for some models.
Contact your local sales office.

Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MELSERVO Others