• No : 23644
  • Release Date : 2018/09/14 15:10
  • Print

Relationship between rotary switch and axis number

What is the relationship between rotary switch of MR-J4-B and axis control number?
Category : 

Answer

When the rotary switch is “0”, the 1st axis and is “1”, the 2nd axis. When the rotary switch is “A”, the 11th axis and is “F”, the 16th axis.
In combination with the auxiliary axis number setting switch, up to 64 axes (MR-J3: 16 axes) can be set.
Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4